AXIS#.IL.PWMFREQ

Description

This parameter provides the current loop PWM frequency for the specified axis.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

kHz

Range

0 to 781.250 kHz

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.PWMFREQ

500ah

2eh

Unsigned32

-

1000:1

Read only

No

AXIS2.IL.PWMFREQ

510ah

2eh

Unsigned32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5823

1

5823 (0x16bf)

AXIS1.IL.PWMFREQ

Unsigned32

Read Only

Yes

71359

2

5823 (0x16bf)

AXIS2.IL.PWMFREQ

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.PWMFREQ

5823

Float

Read Only

-

Related Topics

Current Loop